srio tx from cacheable memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

srio tx from cacheable memory

1,946 Views
s_kalop
Contributor I

Hello.

I use MSC8156ADS board and Spartan 6 connected to it by SRIO. Data transfers go by Ocean DMA succesfully only if memory blocks on MSC8156 is non-cacheable. But if the source address of ocnDMA transfer configuration is set for cacheable memory ocnDMA transmith zeros(digital loopback shows same result). I try to sweep cache for this memory but it is all the same. I see cacheable memory filled with true data while debugging, but ocnDMA transmits zeros.

How can i transmit by ocnDMA from cacheable memory? Thank you.

Tags (1)
0 Kudos
Reply
2 Replies

1,713 Views
yangjie
Contributor II

           os_config.h

#define         num of core      1

 

then  have a try .

 

0 Kudos
Reply

1,713 Views
yangjie
Contributor II

#if (MSC815X_OCN_DMA0 == ON)

ocn_dma_init_params_t ocn_dma_init_params0 =

 

 {

     OCN_DMA_ID0,

     OS_HWI_PRIORITY0,

     {

          /* On which core to enable the channel. */

         ANY_CORE_ID, ANY_CORE_ID, ANY_CORE_ID, ANY_CORE_ID,

      },

     {

              {

                 RIO0_ATMU_BASE,

                 DMA_ATMU_WIN_SIZE,

                 OCN_DMA_INTERFACE_RIO0

              },

           

              {

                  RIO1_ATMU_BASE,

                  DMA_ATMU_WIN_SIZE,

                  OCN_DMA_INTERFACE_RIO1

              },

           

             {

                M3_BASE_ADDR,

                DMA_ATMU_WIN_SIZE,

               OCN_DMA_INTERFACE_LOCAL1

              }

       }

 

 };

 

the OCN-DMA channel depend on core.and cachable data is private for core.you can think about it.

0 Kudos
Reply