sdram on dsp5672x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,896件の閲覧回数
jada
Contributor I

Hello,

I am currently designing a board for the DSP56724 and I want to include some SDRAM. Is there some reference design that shows how to interface the processor with sdrams? The datasheet (or reference manual) shows a configuration where the databus is 24bits and address and data lines are multiplexed. After all a quite unusual configuration so I like to have a look at a working design before I start. I saw somewhere that Freescale is offering a daughterboard for the 56720/4 but I could find a schematic, maybe someone could provide me with a link?

Thanks!

ラベル(2)
タグ(4)
0 件の賞賛
返信
1 解決策
1,631件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Pls refer to the two example code of SDRAM.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,632件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Pls refer to the two example code of SDRAM.

0 件の賞賛
返信