sa606

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

sa606

709 次查看
richt1
Contributor I

Hello,

I am trying to use the SA606D FM IF system in a new design. I have ordered the demo board. The problem is that the recommended parts such as X1 (ICM4712701) are no longer in production. Furthermore, I cannot even find a datasheet so someone else can make an equivalent. Also, Toko has stopped making inductors and a recommended replacement for IFT1 would be helpful. Better yet, a recommended ceramic resonator would be even better. 

Thank you,

Rich

0 项奖励
回复
1 回复

648 次查看
LPP
NXP Employee
NXP Employee

Unfortunately, this has been a problem over the years. Toko and other vendors have made many original adjustable shielded inductors obsolete due to low volume. Coilcraft may have a suitable replacement. Another solution is to use a fixed inductor and large capacitor in parallel with a smaller variable capacitor to provide tuning of the LC tank circuit for the demodulator.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复