requesting for isolated CAN controller IC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

requesting for isolated CAN controller IC

1,058 Views
Nithya_n
Contributor I

Hi Good Afternoon

Can you suggest the Isolated CAN controller IC's , part number for the below requirements mentioned

1) Communication standards - ISO11898-1, ISO11898-2

2) Protocol : CAN2.0B active

3)Format: standard format: ID length 11bit

4)data byte transmission order is big endian

5)Motorola type

6)communication speed:500kbps

7)bit sample point: 72.5 % - 87.5%

8)equipped with high-speed CAN transceiver compliant with ISO11898

9)Terminal resistance:2600ohms.

10)Tolerance shall comply with ISO11898-2

0 Kudos
Reply
1 Reply

1,036 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Nithya,

The only galvanically isolated HS-CAN transceiver in our portfolio is the TJA1052i:

https://www.nxp.com/products/interfaces/can-transceivers/can-with-flexible-data-rate/galvanically-is...

Capture (3).jpgCapture (3).jpg

Capture 1 (2).jpgCapture 1 (2).jpg

Capture 2 (1).jpgCapture 2 (1).jpg

BR, Tomas

0 Kudos
Reply