ptn3460i

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ptn3460i

1,176 Views
mosheben-gigi
Contributor I

How to get PTN3460I FOA & DPCD M TOOL  To Enable change device registers ?

Thanks

Moshe 

0 Kudos
Reply
7 Replies

1,159 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Moshe,

please find the requested FoA and DPCD M tool attached. If password is asked, then enter NXP.

With Best Regards,

Jozef

0 Kudos
Reply

1,147 Views
mosheben-gigi
Contributor I

Many Thaks,

Usind DPCD_M Utility trying Update Register 0x82 "LVDS clock frequency center spreading depth"

With no success 

moshebengigi_0-1756283100287.png

 

Nothing happened Read Data 00 write Data 0x28 Read again 00 

Pls. Advise

Moshe 

0 Kudos
Reply

1,157 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Moshe,

adding DPCD M tool user manual.

With Best Regards,

Jozef

0 Kudos
Reply

1,139 Views
mosheben-gigi
Contributor I

Hi Josef;

Tried exactly as describe, wirte data to register 0x82  (LVDS interface control 2)  

Read 0x82 (Default should be 0x03 ) 0x00 Write 0x2b Read 0x82 0x00, nothing changed 

moshebengigi_0-1756289068647.png

moshebengigi_2-1756289114385.png

 

 

Tags (1)
0 Kudos
Reply

1,133 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Moshe,

thank you for the printscreens. If the firmware versions are F6 and F4, you either have the PTN3460BS version, or you have incorrect Firmware versions loaded in the PTN3460IBS. Please check the top marking of your chip. To find out which PTN3460 version you have. Or please take a picture of the top marking and please share the picture with visible lines. 

Latest Firmware version for the PTN3460IBS is F2. For the PTN3460BS, it is F6. Please refer to the release notes attached. 

Please make sure you follow the correct programming guide (although the 0x82 is the same register in both). 

With Best Regards,

Jozef

0 Kudos
Reply

1,123 Views
mosheben-gigi
Contributor I

Hi,

First, thank you for the document describing the differences between the firmware versions. Due to a misunderstanding, I flashed version F6 thinking it was more advanced. The component in use is PTN3460IBS. I then re-flashed version F2, but unfortunately, the result was the same — writing to the address 0x82 Data 0x23 read back 0x00 

moshebengigi_0-1756291904820.png

 

moshebengigi_1-1756291952786.png

 

moshebengigi_2-1756291989775.pngmoshebengigi_3-1756292022311.png

 

0 Kudos
Reply

971 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Moshe,

I have found an older case, where another customer asked similar question. Please see the answer. 

  • DPCD M Tool is designed for PTN3355BS, not PTN3460I.
  • PTN3460I does not expose its configuration registers via DPCD.
  • You must use I2C or AUX channel commands for PTN3460I.

For the I2C, please make sure it is set as slave with DEV_CFG open or connected to GND, that you will use correct I2C address. 

Screenshot_1.png

I apologize for inconvenience. 

With Best Regards,

Jozef

0 Kudos
Reply