problem: wire ack fault - target connected?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem: wire ack fault - target connected?

3,446件の閲覧回数
yvzblgcyln
Contributor I

Hi, i have a problem which says "wire ack fault - target connected?" while debuging. Is there any suggestion to solve it?

I am using LPC-Link 2 and CLEV6630A board. That issue occurs when i try to debug "NfcrdlibEx4_MIFAREClassic" example which published by NXP itselfs.

Tnx for now, have good day y'all.

yvzblgcyln_0-1642140886308.png

 

0 件の賞賛
返信
7 返答(返信)

3,429件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @yvzblgcyln :

CLEV6630A evaluation board needs to be connected to the computer via LPC-Link2, as shown  below.

danielchen_0-1642339837586.png

 

Please also check the LPC firmware and driver.  you can refer to chapter 3 in AN11022:  CLRC663 Evaluation board quick start guide.

https://www.nxp.com.cn/docs/en/application-note/AN11022.pdf

 

Regards

Daniel

  

 

3,413件の閲覧回数
yvzblgcyln
Contributor I

Thanks for your reply, my connection looks similar as in picture. I also checked quick start guide, there is nothing i didn't do.

0 件の賞賛
返信

3,398件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @yvzblgcyln :

please check the device manager of your pc, there should have a J-link driver.

danielchen_1-1642425060018.png

If this J-link driver exists, please use jlink commands to check this connection is successful, please refer to  below picture.

danielchen_0-1642424934992.png

 

 

Regards

Daniel

 

0 件の賞賛
返信

3,395件の閲覧回数
yvzblgcyln
Contributor I

Hi, there is a J-link driver in device manager as you sent. Then i checked my connection, at the end of process J-Link commender said "Cannot connect to target". What am i suppose to do?

I don't know why but i do not have permission to upload images. Here is my J-Link commender script's output:

SEGGER J-Link Commander V7.60c (Compiled Jan 7 2022 16:10:33)
DLL version V7.60c, compiled Jan 7 2022 16:09:18

Connecting to J-Link via USB...O.K.
Firmware: J-Link LPC-Link 2 compiled Apr 4 2019 16:55:05
Hardware version: V1.00
S/N: 611000000
VTref=3.300V


Type "connect" to establish a target connection, '?' for help
J-Link>connect
Please specify device / core. <Default>: LPC1769
Type '?' for selection dialog
Device>
Please specify target interface:
J) JTAG (Default)
S) SWD
T) cJTAG
TIF>s
Specify target interface speed [kHz]. <Default>: 4000 kHz
Speed>
Device "LPC1769" selected.


Connecting to target via SWD
Cannot connect to target.
J-Link>

0 件の賞賛
返信

3,380件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

I would suggest you change another j-link or LPC link,   or try this lpc-link with another board.

Did you rework this board?  for example ,remove some components from this board? Did this board work before?

 

Regards

Daniel

 

0 件の賞賛
返信

3,377件の閲覧回数
yvzblgcyln
Contributor I

Hi, this card was working 2 mounths ago. My coworker was working on it, and last time he gave it, i guess it was working. I just connected cables (LPC-Link:J7 to CLEV6630A and other USB cables), i didn't change anything on it. Also i have just one LPC-Link and one board. 

0 件の賞賛
返信

3,357件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

 

I would suggest you check the power supply. make sure the jumpers are in the right places according to the quick start guider.

danielchen_0-1642571935492.png

J-link is in the right direction.  

 

Regards

Daniel

 

0 件の賞賛
返信