pn7161 and mobiles phone

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pn7161 and mobiles phone

64件の閲覧回数
user_ahmed
Contributor II

Hi

am I need a third-party application (such as an NFC app from the Play Store) to enable peer-to-peer communication on Android. or IPHONE  

 

or if i have third party application i cant use p2p on all phones 

0 件の賞賛
返信
2 返答(返信)

26件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @user_ahmed 

PN7160 supports P2P feature between the two PN7160 devices, does not support  P2P feature between PN7160 and Android, because P2P feature has been removed onwards Android 12.

 

 

0 件の賞賛
返信

14件の閲覧回数
user_ahmed
Contributor II

even i use  mobile application to read or write nfc 

not work in peer to peer mode after android 12  or iphone ?

タグ(1)
0 件の賞賛
返信