mpc5121 linux boot via nfs not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mpc5121 linux boot via nfs not working

跳至解决方案
4,131 次查看
kbm1008
Contributor I

I'm new to LTIB.  I'm having trouble getting an nfs mount of my rootfs to work.   I followed the instructions in AN3765: Porting Linux for the MPC5121e, Appendix B.  Linux boot using "run net_nfs" fails with an "nfs: server 192.168.1.32 not responding" error.  I then tried to simply mount the rootfs manually and that fails with a "Protocol not supported" error.  Both host and target have fixed IP addresses.  Specifics:

 

host/nfs_server: 192.168.1.32

target: 192.168.1.45

 

host>cd /tftpboot 

host>ls -l ltib
lrwxrwxrwx 1 brenda brenda 24 2009-04-20 14:16 ltib -> /home/brenda/ltib/rootfs

host>exportfs

/home/brenda/ltib-mpc5121ads-20081208/rootfs
                192.168.1.45

 

target>mount 192.168.1.32:/tftpboot/ltib /mnt
mount: mounting 192.168.1.32:/tftpboot/ltib on /mnt failed: Protocol not supported

 

The host syslog simply shows that mountd authenticated a mount request from 192.168.1.45.  I've been trying to figure out what the "Protocol not supported" error means with no luck.  Any help appreciated.

 

0 项奖励
回复
1 解答
2,324 次查看
kbm1008
Contributor I

Fabio - thanks for the reply.  I finally figured out what was going on.  We recently had to move some hardware to a different subnet including both the 5121 board and the host computer.  And while I had set the new IP address both in U-boot environment variables and directly on the Linux installed on the board, I had forgotton that I configured the board address in ltib before the hdwe move.  Which explains why the new rootfs could not be mounted by NFS (address was changing during the boot process).  Still doesn't explain why a manual mount command didn't work since the host /etc/exports file and board had the new address.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,324 次查看
fabio_estevam
NXP Employee
NXP Employee

Try to mount the /tftpboot/ltib directory on your host PC first.

 

Make sure you have NFS installed and running and that you added an entry for /tftpboot/ltib into /cat/exports

 

Regards,

 

Fabio Estevam

0 项奖励
回复
2,325 次查看
kbm1008
Contributor I

Fabio - thanks for the reply.  I finally figured out what was going on.  We recently had to move some hardware to a different subnet including both the 5121 board and the host computer.  And while I had set the new IP address both in U-boot environment variables and directly on the Linux installed on the board, I had forgotton that I configured the board address in ltib before the hdwe move.  Which explains why the new rootfs could not be mounted by NFS (address was changing during the boot process).  Still doesn't explain why a manual mount command didn't work since the host /etc/exports file and board had the new address.

0 项奖励
回复
2,324 次查看
bbjh1
Contributor I

Hi I am facing the same problem. I installed and configured ltib for mpc5121e on my host. How can I mount the imgae using tftp?

0 项奖励
回复
2,324 次查看
hpdwally
Contributor II

I run a  little script before I boot ubuntu to get the NFS server working

 

 

sudo ifconfig eth3 172.27.27.100 netmask 255.255.255.0

sudo dpkg-reconfigure portmap

sudo /etc/init.d/portmap restart

sudo /etc/init.d/xinetd restart

sudo /etc/init.d/nfs-kernel-server restart

 

Make sure you do not bind to the local loopback, that caught me off for a day or so >:

0 项奖励
回复