lx2160ardb Xspi-fw add tiny.itb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lx2160ardb Xspi-fw add tiny.itb

1,018 Views
wutianyi
Contributor II

Hi  NXP:

    We found a strange issue while building SPI-firmware. If I don't put tiny images in the back, then this firmware will work. If I put Tiny image, it won't boot. This problem is very strange, according to the data behind, it will not affect the normal boot logic.

This is my makefile:

define fcreate_boot
$(Q)dd if=$(IMAGE_BUILD)/$(PBL_BIN) of=$(IMAGE_BUILD)/boot.bin
$(Q)dd if=$(IMAGE_BUILD)/$(FIP_BIN) of=$(IMAGE_BUILD)/boot.bin seek=1 bs=1M
$(Q)dd if=$(IMAGE_BUILD)/$(DDR_BIN) of=$(IMAGE_BUILD)/boot.bin seek=1 bs=8M
$(Q)dd if=$(IMAGE_BUILD)/$(MC_IMG) of=$(IMAGE_BUILD)/boot.bin seek=1 bs=10M
$(Q)dd if=$(IMAGE_BUILD)/dpl.dtb of=$(IMAGE_BUILD)/boot.bin seek=1 bs=13M
$(Q)dd if=$(IMAGE_BUILD)/dpc.dtb of=$(IMAGE_BUILD)/boot.bin seek=1 bs=14M
#$(Q)dd if=$(IMAGE_BUILD)/$(LINUX_DTB) of=$(IMAGE_BUILD)/boot.bin seek=1 bs=15M
#$(Q)dd if=$(IMAGE_BUILD)/linux.itb of=$(IMAGE_BUILD)/boot.bin seek=1 bs=16M
endef

Thanks

Tianyi

Labels (1)
0 Kudos
Reply
2 Replies

989 Views
yipingwang
NXP TechSupport
NXP TechSupport

dd if=${DEPLOY_DIR_IMAGE}/${img_file} of=${fw_img} bs=1K seek=${offset}

seek should be offset of the image.

For memory map, please refer to "Table 22. Unified 64 MiB memory layout of NOR/QSPI/XSPI/NAND/SD media for composite firmware on all Layerscape platforms" in LSDK 21.08 user manual.

986 Views
wutianyi
Contributor II

Thank you. I've identified the problem. There is no problem in the img production, because the case of flash configured inside the driver is wrong, the actual flash is 32M, and the driver configuration is 64M. The hardware does not support such a large image.

Thanks

Tianyi

0 Kudos
Reply