iMX8MM Disk encryption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MM Disk encryption

Jump to solution
1,130 Views
richardmarsh
Contributor I

I have read AN12714 and would like to try this out on a more up to date version of the kernel (5.10 or later).

The patch files referenced in the imx_sec_apps/meta-imx-fde-demo layer do not apply to later kernels.

Are the patches even required now or can the same behaviour be achieved using a standard linux-imx kernel?

My ultimate goal is to encrypt a file/partition using a key derived using a CMK to ensure confidentiality and resilience against outside influence.

Thanks,

Richard

0 Kudos
Reply
1 Solution
1,110 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The latest kernel and bsp include the patches on it, you don't need install anything.

Regards

View solution in original post

0 Kudos
Reply
1 Reply
1,111 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The latest kernel and bsp include the patches on it, you don't need install anything.

Regards

0 Kudos
Reply