i.MX Forums i.MX RT Command line compiling for RT1176

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX Forums i.MX RT Command line compiling for RT1176

跳至解决方案
3,576 次查看
MN19000
Contributor III

i.MX Forums i.MX RT

I am using MIMXRT1170 MCU.

I need to compile my project from command line. Please send me instruction

0 项奖励
回复
1 解答
3,455 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @MN19000

From the batch file you share, I see you are using a different path for the toolchain and for the IDE you are using. Please update the path to: "C:\nxp\MCUXpressoIDE_11.7.1_9221\ide\tools\bin" to make it match with the IDE version you are using.

Please try this and let me know if the issue persists.

BR,
Edwin.

在原帖中查看解决方案

4 回复数
3,559 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @MN19000,

Please look into the following post, as I believe it might just be what you are looking for!

https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-li...

BR,
Edwin.

0 项奖励
回复
3,510 次查看
MN19000
Contributor III

Hi @EdwinHz 

I have used an example code, but it is failing due to launching Eclipse IDE.
Here is the batch file
 
-------------
 

# Batch file to build an Eclipse project from the command line on Windows

# Example for using MCUXpresso IDE
 
# path to GNU tools and compiler: arm-none-eabi-gcc.exe, ....
SET TOOLCHAIN_PATH=C:\nxp\MCUXpressoIDE_10.0.2_411\ide\tools\bin
 
# variable to the command line Eclipse IDE executable
SET IDE=C:\nxp\MCUXpressoIDE_11.7.1_9221\ide\mcuxpressoidec.exe
 
ECHO Extending PATH if not already present
ECHO %PATH%|findstr /i /c:"%TOOLCHAIN_PATH:"=%">nul || set PATH=%PATH%;%TOOLCHAIN_PATH%
 
ECHO Launching Eclipse IDE

"%IDE%" -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "c:\tmp\wsp" -build evkmimxrt1170_freertos_event_cm7

I have followed the instruction  on the link, but it is still not working
 
WARNING: No Project matched "evkmimxrt1170_freertos_event_cm7". Skipping...
 
-----------
C:\CL_NXP\CommandLine_Test>ECHO Launching Eclipse IDE
Launching Eclipse IDE
 
C:\CL_NXP\CommandLine_Test>"C:\nxp\MCUXpressoIDE_11.7.1_9221\ide\mcuxpressoidec.exe" -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "c:\tmp\wsp" -build evkmimxrt1170_freertos_event_cm7
SLF4J: Failed to load class "org.slf4j.impl.StaticLoggerBinder".
SLF4J: Defaulting to no-operation (NOP) logger implementation
WARNING: No Project matched "evkmimxrt1170_freertos_event_cm7". Skipping...
===========
0 项奖励
回复
3,456 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @MN19000

From the batch file you share, I see you are using a different path for the toolchain and for the IDE you are using. Please update the path to: "C:\nxp\MCUXpressoIDE_11.7.1_9221\ide\tools\bin" to make it match with the IDE version you are using.

Please try this and let me know if the issue persists.

BR,
Edwin.

3,417 次查看
MN19000
Contributor III
Thank you, that solved my issue.
0 项奖励
回复