hi,
i have a processor freescale mc9s12. i want upload firmware to this processor. how can i do, i dont know. How do I enable communication with the PC. Which should I use communication protocol? which i use comminication device?
解決済! 解決策の投稿を見る。
If you already have .s19 or .elf file, you can also use hiwave.exe tool included in CodeWarrior to program flash. CodeWarrior v5.1 can be downloaded from:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X
The method is as below:
1. Install Codewarrior.
2. make sure the hardware is well connected with PC. For instance you are using BDM multilink or Cyclone Pro.
3. open Hiwave debugger “Hiwave.exe” in {Your CW install directory}\prog
4. then in debugger, go to menu “component”, “set connection…”. In new pop-up small dialog, in the dropdown list, select HC12 and P&E Multilink/Cyclone Pro. Click OK to close this dialog.
5. go to menu “MultilinkCyclonePro”, “device”, select the right device chip.
6. go to menu “MultilinkCyclonePro”, “connect”, Set the right connection.
7. go to menu “File”, “Load application…”. Import the .s19 or .elf file into debugger. You could have a browse the content at the memory window of the debugger, it should be in coincidence with the s-record file.
8. Press F5 to run. The code should download into the flash.
Freescale has no stand-alone software for flash programmer, if you need a standalone tool, you may choose the one supplied by P&E:
http://tinyurl.com/7ugmbuo
It supports P&E Multilink.
Fiona Kuang
Technical Information & Commercial Support
If you already have .s19 or .elf file, you can also use hiwave.exe tool included in CodeWarrior to program flash. CodeWarrior v5.1 can be downloaded from:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X
The method is as below:
1. Install Codewarrior.
2. make sure the hardware is well connected with PC. For instance you are using BDM multilink or Cyclone Pro.
3. open Hiwave debugger “Hiwave.exe” in {Your CW install directory}\prog
4. then in debugger, go to menu “component”, “set connection…”. In new pop-up small dialog, in the dropdown list, select HC12 and P&E Multilink/Cyclone Pro. Click OK to close this dialog.
5. go to menu “MultilinkCyclonePro”, “device”, select the right device chip.
6. go to menu “MultilinkCyclonePro”, “connect”, Set the right connection.
7. go to menu “File”, “Load application…”. Import the .s19 or .elf file into debugger. You could have a browse the content at the memory window of the debugger, it should be in coincidence with the s-record file.
8. Press F5 to run. The code should download into the flash.
Freescale has no stand-alone software for flash programmer, if you need a standalone tool, you may choose the one supplied by P&E:
http://tinyurl.com/7ugmbuo
It supports P&E Multilink.
Fiona Kuang
Technical Information & Commercial Support
Hello recep,
Which board do you use ? Or what is the chip part number ?
And which IDE do you use ?
BR
Alice