how to modify wct-5wtxauto for 1-coil system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to modify wct-5wtxauto for 1-coil system

1,114 Views
devinpark
Contributor II

Hi,

WCT-5WTXAUTO is a 5w 3-coil tx charger. BTW, I want to make a 1-coil tx charger 

 

On the side of HW, some unnecessary blocks would be able to be removed : coil selection-related TR, etc... 

 

Then how about SW-side? I'm using SDK4.0. I found some coil-related variables.

 

      #define NUM_COILS_PER_DEVICE                    1u//3u

And then, I modified following ARRAY variables which controlled 3 coils originally. 

   BYTE byCoilIds[NUM_DEVICES][NUM_COILS_PER_DEVICE] = {{ 0u } }; //{2,1,0};         // set coil combinations by customer

   #define PWM_CHANNEL_MAPPING                     { 3u }//{ 3u, 3u, 3u }

   #define COIL_ENABLE_CONTROL_PORTS               { (STANDARD_REGISTER_SIZE *) &GPIOC_DR, }

   #define COIL_ENABLE_CONTROL_BIT_MASKS           { 0x2000u}

   #define COIL_DISCHARGE_CONTROL_PORTS            { (STANDARD_REGISTER_SIZE *) &GPIOB_DR }

   #define COIL_DISCHARGE_CONTROL_BIT_MASKS        { 0x80u}

And also  EEdata_FlashDefaults.asm was modified to have only 1 coil parameters..

I wonder if it's enough for 1-coil migration. .

Pls help me if you have any experience on it.

Thanks & BR,

Devin

 

Labels (1)
0 Kudos
Reply
1 Reply

983 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Devin,

 

For Single Coil design, I rather recommend you to use the WCT-15WTX1COILFF which is a single-coil fixed frequency wireless charging transmitter reference design uses the WCT10xx transmitter controller IC that integrates all required functions for the Wireless Power Consortium (WPC) Qi-compliant wireless power transmitter design.

 

Currently, the design is under preproduction, but you can access some documentation with a signed NDA with your distributor.

 

Regards,

Jose

0 Kudos
Reply