how to choose the emmc for LS1043A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to choose the emmc for LS1043A

Jump to solution
3,426 Views
manid
Contributor I

Hi

we are developing the LS1043A processor. and booting option is eMMC . 

LS1043A support eMMC up to rev 4.4/4.5, but eMMC 4.4 and 4.5 has been discontinued and some 4.4 and 4.5 eMMC component  is obsolete. If I should use the 5.0 or upper version eMMC, on what basis I can select high version of eMMC?

 

if i select the higher version how to use the data strobe pin?

 

0 Kudos
Reply
1 Solution
3,410 Views
Pavel
NXP Employee
NXP Employee

The LS1043a eSDHC can use this eMMC, since eMMC devices version 5.0 and higher are backward compatible to previous versions.

View solution in original post

0 Kudos
Reply
6 Replies
3,267 Views
manid
Contributor I

is LS1043 support HS200 mode with 4 bit mode?? 

0 Kudos
Reply
3,411 Views
Pavel
NXP Employee
NXP Employee

The LS1043a eSDHC can use this eMMC, since eMMC devices version 5.0 and higher are backward compatible to previous versions.

0 Kudos
Reply
3,405 Views
manid
Contributor I

HI

The latest emmc ver 5.0 and 5.1 have data strobe and reset pin. but LS1043A don't have these pin. how configure these pin??

0 Kudos
Reply
3,380 Views
Pavel
NXP Employee
NXP Employee

The Data strobe signal is used in HS400mode. The LS1043a does not support this mode.

There is internal pull-up on reset in eMMC ver 5.0 and 5.1.

It is not necessary to put pull-up resistance on RST_n (H/W rest) line if host does not use H/W reset. 

0 Kudos
Reply
3,376 Views
manid
Contributor I

is LS1043A support HS200 mode??

0 Kudos
Reply
3,349 Views
Pavel
NXP Employee
NXP Employee

Yes, the LS1043a eSDHC supports HS200 mode. See the Section 22.1.1 in the LS1043a Reference Manual.

0 Kudos
Reply