help!!!!!!!!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

help!!!!!!!!!

2,249件の閲覧回数
sup
Contributor I
my board use NAND flash K9F1G08R0A . but redboot can not work. who can tell me where to set redboot working nand flash boot .
0 件の賞賛
返信
2 返答(返信)

1,327件の閲覧回数
Vannes
Contributor I

Just a little description, no more?

How do we HELP you?

0 件の賞賛
返信

1,327件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee
It's hard to tell what is wrong with the amount of information you provided.
 
We could better understand your problem if you have more information like:
 
- What hardware are you using?
 
- Are you using ATK to flash your board? If so, which version?
 
- What is the error you get?
 
- Can you try to erase the NAND flash and program Redboot?
 
Regards,
 
Fabio Estevam
0 件の賞賛
返信