help!!!!!!!!!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

help!!!!!!!!!

2,261 Views
sup
Contributor I
my board use NAND flash K9F1G08R0A . but redboot can not work. who can tell me where to set redboot working nand flash boot .
0 Kudos
Reply
2 Replies

1,339 Views
Vannes
Contributor I

Just a little description, no more?

How do we HELP you?

0 Kudos
Reply

1,339 Views
fabio_estevam
NXP Employee
NXP Employee
It's hard to tell what is wrong with the amount of information you provided.
 
We could better understand your problem if you have more information like:
 
- What hardware are you using?
 
- Are you using ATK to flash your board? If so, which version?
 
- What is the error you get?
 
- Can you try to erase the NAND flash and program Redboot?
 
Regards,
 
Fabio Estevam
0 Kudos
Reply