gstreamer vpu plugins and qt on imx27

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

gstreamer vpu plugins and qt on imx27

2,200件の閲覧回数
xpc
Contributor I

Hello,

I have to create a Qt-embedded application, which plays video file, using the vpu plugins of gstreamer on i.mx27, without X server.

But it seems that there is no gstreamer video sink, compatible with qt-embedded.

 

As I understood, the phonon multimedia framework, works with gstreamer. But obviously it does not give the opportunity gstreamer to work with certain plugins, such as the vpu encoder/decoder.

 

Can someone give me any ideas, how to integrate gstreamer with vpu plugins in a Qt-embedded application?

 

Thanks in advance,

H. Tsenov

 

0 件の賞賛
返信
2 返答(返信)

994件の閲覧回数
jf_nicolas
Contributor I

Hello,

 

I'm facing excatly the same issue.

Did you find any solution to this problem ?

 

Thanks in advance.

0 件の賞賛
返信

994件の閲覧回数
jviguera
Contributor I

Hi all,

 

Exactly the same problem here on an i.mx51.

 

Did anyone of you of anyone in the forum find a solution/clue?

 

Please, any idea posted in the forum would be appreciated.

 

--

Regards,

 

Javier Viguera

 

 

 

0 件の賞賛
返信