flexray ID

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

flexray ID

2,231 次查看
sdm
Contributor I

MC9S12XF542MLM在做flexray传输时该怎样修改静态段和动态段的ID范围以及最大数据长度?谢谢!

0 项奖励
回复
1 回复

2,209 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

 

FlexRay allows many configuration options and at the same time the individual configuration parameters are quite interconnected. If the customer sends a request that he wants to send in slot 100 and at the same time the payload needs to be changed, it means to make a new configuration of the communication cycle, which already requires some knowledge of the FlexRay protocol.

 

We can try to answer the following, where we will outline what the customer should change, but if the customer does not understand the FlaxRay protocol, it will be very difficult with any additional support.

 

FlexRay configuration is very variable and you can adopt communication cycle exactly for your purposes but this requires more detailed knowledge of the FlexRay Protocol specification. Thus we can provide you basic information how the communication cycle used in our FlexRay UNIFIED driver example is configured:

 

Unified Driver is configured as follows: (Please, see, Fr_UNIFIED_cfg.c file where you can find yellow labeled configuration parameters.)

 

gdCycle=5ms (G_MACRO_PER_CYCLE=5000)

gdStaticSegment=(G_NUMBER_STATIC_SLOTS * GD_STATIC_SLOT)=60*50=3000 (3ms)

gdDynamicSegment=(G_NUMBER_OF_MINISLOTS * GD_MINISLOT)=22*40=880

gdSymbolWindow=(GD_SYMBOL_WINDOW)=13

gdNIT=gdCycle-(gdStaticSegment+gdDynaicSegment+gdSymbolWindow)=5000-(3000+880+13)=1107

 

In our example Frames IDs <1,60> will be transmitted in static segment and Frames IDs <61,82> in dynamic segment.

 

 

lama_0-1650375185610.png

 

 

 

“How to change the ID range?”

  • You can change either G_NUMBER_STATIC_SLOTS or G_NUMBER_OF_MINISLOTS depending on used segment, but you must ensure that equation above is always valid!
  •  

“How to change data length of data in static and dynamic segment?

  • Static segment -  change G_PAYLOAD_LENGTH_STATIC configuration parameter and please see FlexRay Protocol Specification for more details. Caution! This parameter is limited by GD_STATIC_SLOT parameter.
  • Dynamic Segment – change P_PAYLOAD_LENGTH_DYN_MAX and please see FlexRay Protocol Specification for more details.

 

Caution! Configuration parameters with G_ & GD_ prefixes must be changed in all FlexRay nodes connected to one cluster!!!

Best regards,

Ladislav

 

0 项奖励
回复