ecspi 1 for spi eeprom is not working on imx8mq

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ecspi 1 for spi eeprom is not working on imx8mq

2,980 次查看
krupa_parameswa
Contributor I

Hello 

I am using imx8mq processor based evk where i am trying to configure spi eeprom on ecspi 1 but unable to get clock signal when probed but the driver is getting register, plz someone help me out in solving this issue why i am unable to use ecspi as expected.

The following is been configured in dts file:

ecspi1: ecspi@30820000 {
compatible = "fsl,imx6ul-ecspi", "fsl,imx51-ecspi";
reg = <0x0 0x30820000 0x0 0x10000>;
interrupts = <GIC_SPI 31 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_ECSPI1_ROOT>,
<&clk IMX8MQ_CLK_ECSPI1_ROOT>;
clock-names = "ipg", "per";
interrupt-parent = <&gpc>;
fsl,spi-num-chipselects = <1>;
cs-gpios = <&gpio5 9 0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi1>;
#address-cells = <1>;
#size-cells = <0>;
status = "okay";

/* MAGIK2_SMARC : Secure EEPROM */
eeprom: ataes132a@0 {
compatible = "atmel,at25";
reg = <0>;
size = <65536>;
pagesize= <32>;
address-width= <16>;
spi-max-frequency = <1000000>;
};

pinctrl_ecspi1: ecspi1grp {
fsl,pins = <
/* MAGIK2_SMARC : TBC whether to configure SS0 as GPIO ALT mode or ECSPI1_SS0 mode */
/*MX8MQ_IOMUXC_ECSPI1_SS0_ECSPI1_SS0 0x100b1*/
MX8MQ_IOMUXC_ECSPI1_SS0_GPIO5_IO9 0x19
MX8MQ_IOMUXC_ECSPI1_MISO_ECSPI1_MISO 0x100b1
MX8MQ_IOMUXC_ECSPI1_MOSI_ECSPI1_MOSI 0x100b1
MX8MQ_IOMUXC_ECSPI1_SCLK_ECSPI1_SCLK 0x100b1
>;
};

Regards

Krupa

标记 (1)
0 项奖励
回复
3 回复数

2,590 次查看
krupa_parameswa
Contributor I

Hello igor

In our configuration uart3 is configured in the below way

pinctrl_uart3: uart3grp {
fsl,pins = <
MX8MQ_IOMUXC_UART3_TXD_UART3_DCE_TX 0x49
MX8MQ_IOMUXC_UART3_RXD_UART3_DCE_RX 0x49
>;
};

 where we are not using SPI lines for that 

And MX8MQ_IOMUXC_ECSPI1_SCLK this lines we are not using for mip-dsi 

still we are unable to get clock signal when probes , please can you tell is there any other way to configure to use spi eeprom

Regards

Krupa

0 项奖励
回复

2,590 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Krupa

one can look at nitrogen 8m ecspi2 example:

linux-imx6/imx8mq-nitrogen8m.dts at boundary-imx_4.9.x_8mq_ga-pass1-ath10k · boundarydevices/linux-i... 

Best regards
igor

0 项奖励
回复

2,589 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Krupa

one can try latest Linux L4.14.78 and check that some ecspi1 pins

are used by other modules, for example MX8MQ_IOMUXC_ECSPI1_MISO*,

MX8MQ_IOMUXC_ECSPI1_SS0* are used by uart3
and MX8MQ_IOMUXC_ECSPI1_SCLK* by mipi-dsi in fsl-imx8mq-evk.dts,
fsl-imx8mq-evk-lcdif-rm67191.dtsi

freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

For testing one can use spi unit test

mxc_spi_test\test - imx-test - i.MX Driver Test Application Software 

Just for reference one can look at sect.4.3 Enhanced Configurable Serial Peripheral

Interface (ECSPI) attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复