delayed pwm output 56f8323

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

delayed pwm output 56f8323

2,262 Views
arjan
Contributor I
hi,

i want to generate four pwm sigals, of which two are delayed with respect to the other two.
How can i do this, since all pwm ouputs are based on the same counter?

thanks in advance,

arjan
0 Kudos
Reply
2 Replies

1,113 Views
mr_venkatarao
Contributor I
hi, i don't know which is your mcu.
but start the timer after intialisation of all 4 pwm functions instead of starting before.I did the same in power pc (mpc55540 mcu.
0 Kudos
Reply

1,113 Views
Alban
Senior Contributor II
Hello Power PC,

The device is in the subject line. It is 56F8323.
I think it is a DSP, I don't work with these for now.

Alban.
0 Kudos
Reply