delayed pwm output 56f8323

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

delayed pwm output 56f8323

2,244件の閲覧回数
arjan
Contributor I
hi,

i want to generate four pwm sigals, of which two are delayed with respect to the other two.
How can i do this, since all pwm ouputs are based on the same counter?

thanks in advance,

arjan
0 件の賞賛
返信
2 返答(返信)

1,095件の閲覧回数
mr_venkatarao
Contributor I
hi, i don't know which is your mcu.
but start the timer after intialisation of all 4 pwm functions instead of starting before.I did the same in power pc (mpc55540 mcu.
0 件の賞賛
返信

1,095件の閲覧回数
Alban
Senior Contributor II
Hello Power PC,

The device is in the subject line. It is 56F8323.
I think it is a DSP, I don't work with these for now.

Alban.
0 件の賞賛
返信