cannot read the data from external memory in mucu like S32R45 etc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cannot read the data from external memory in mucu like S32R45 etc

1,027 Views
HyunungPark
Contributor III

I know that the clock is different when HSM works or MCU like the S32R45.

so the function of crypto works normally.

But any data cannot be read from external memory.

what is the solution to resolve this issue?

Hyunung Park

0 Kudos
Reply
2 Replies

1,016 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you please specify the issue closer?

S32R45 does not have HSM.

But any data cannot be read from external memory.

What data? What configuration? Which SW is used to do so? etc..

Also please state name of company, in case I have to ask internally for help, this is required.

Best regards,

Peter

0 Kudos
Reply

989 Views
HyunungPark
Contributor III

Hi

This issue is resolved.

BRs.

  • Hyunung Park
0 Kudos
Reply