bus fault: difference between 2 the same processors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bus fault: difference between 2 the same processors

905 Views
mh3
Contributor I

Hello NXP,

I have received my second batch of hardware with the k64f processor on it. However i notice a difference between the first batch and the second batch. The first one runs the software and the second one immediately gets a BUS FAULT. You would say a hardware error but a sample project works like a charm. (dhcp4_client) What could cause the difference between the first batch and the second batch?


<err> os: ***** BUS FAULT *****
<err> os: Precise data bus error
<err> os: BFAR Address: 0x4003d014
<err> os: r0/a1: 0x4003d000 r1/a2: 0x2000f61c r2/a3: 0x4003d000
<err> os: r3/a4: 0x68000201 r12/ip: 0x00000777 r14/lr: 0x00014e9d
<err> os: xpsr: 0x61000000
<err> os: s[ 0]: 0x00000000 s[ 1]: 0x00025064 s[ 2]: 0x20000b78 s[ 3]: 0x00023285
<err> os: s[ 4]: 0x00000401 s[ 5]: 0x00000000 s[ 6]: 0x00000000 s[ 7]: 0x00000000
<err> os: s[ 8]: 0x00024efc s[ 9]: 0x00025064 s[10]: 0x00024efc s[11]: 0x0002423f
<err> os: s[12]: 0x00024ed4 s[13]: 0x00015733 s[14]: 0x2000acdd s[15]: 0x00025364
<err> os: fpscr: 0x00025364
<err> os: Faulting instruction address (r15/pc): 0x00023bc4
<err> os: >>> ZEPHYR FATAL ERROR 25: Unknown error on CPU 0
<err> os: Current thread: 0x20004d78 (unknown)
<err> os: Halting system

and the project config:

# Basic networking
CONFIG_NETWORKING=y
CONFIG_NET_IPV4=y
CONFIG_NET_IPV6=n
CONFIG_NET_TCP=y
CONFIG_NET_ARP=y
CONFIG_NET_UDP=y
CONFIG_DNS_RESOLVER=y

# MQTT
CONFIG_MQTT_LIB_TLS=n
CONFIG_MQTT_LIB=y
CONFIG_NET_SOCKETS=y
CONFIG_POSIX_API=y
CONFIG_JSON_LIBRARY=y
CONFIG_NEWLIB_LIBC=y
CONFIG_NEWLIB_LIBC_FLOAT_PRINTF=y
CONFIG_FPU=y

#memory
CONFIG_MAIN_STACK_SIZE=8192

# Network buffers
CONFIG_NET_BUF_RX_COUNT=64
CONFIG_NET_BUF_TX_COUNT=64
CONFIG_NET_PKT_RX_COUNT=64
CONFIG_NET_PKT_TX_COUNT=64

# DHCP specific configurations
CONFIG_NET_DHCPV4=y
CONFIG_NET_DHCPV4_OPTION_CALLBACKS=y

# Network management
CONFIG_NET_MGMT=y
CONFIG_NET_MGMT_EVENT=y

# Logging
CONFIG_LOG=y
CONFIG_NET_LOG=y

# Random number generation for MQTT message IDs
CONFIG_ENTROPY_GENERATOR=y
CONFIG_TEST_RANDOM_GENERATOR=y

#timers
CONFIG_COUNTER=y

#miscelanious
CONFIG_GPIO=y
CONFIG_SPI=n
CONFIG_SPI_ASYNC=n
CONFIG_ADC=y
CONFIG_JSON_LIBRARY=y
Tags (2)
0 Kudos
Reply
1 Reply

874 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @mh3 ,

Thanks for your post.

To help you figure out the issue more accurately, could you please provide more information? You mentioned that you received two batches of K64 processors. Would it be convenient for you to tell me the receipt times of these two batches? Also, could you provide me with the mask information printed on the chips of these two batches? You can take photos like this.

 
 

Image (14).jpg

 

Apart from the dhcp4_client encountering a bus fault on the second batch processors, have you tried other SDK demos? Do they also occur bus faults? In the second batch processors, does only a certain chip have a bus fault, or do all of them have this problem?

BRs,

Celeste

0 Kudos
Reply