bga3031

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bga3031

1,494 Views
darren1
Contributor I

Don't know if I am in the right place for start, or belong here, I only wanted to ask a question to nxp but here I am in a forum.

I have bought from Amazon an amplifier board based on the bga3031 for SDR usage. I think it is maybe not suitable (out of the box) and apparently needs to be controlled via an SPI interface. The seller I think is based in China and despite their claims to produce arduino (STM32) code "on request" ... it ain't happening I think. I am not an "electronics or programming guy", so is there some code somewhere out there?

Thank you all in advance.

Labels (1)
  • RF

Tags (2)
0 Kudos
Reply
1 Reply

1,407 Views
andrei_skok
NXP Employee
NXP Employee

NXP offers the BGA3X31 evaluation kit OM17024: DOCSIS 3.1 upstream amplifier BGA3131 customer evaluation kit|NXP .

Kit Contains:


RF evaluation board
USB interface board
Flat cable
Samples
USB flash driver containing: evaluation software, Introduction etc.
ESD safe casing

I am nor sure what bga3031 board you have but we support only our products.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------