Don't know if I am in the right place for start, or belong here, I only wanted to ask a question to nxp but here I am in a forum.
I have bought from Amazon an amplifier board based on the bga3031 for SDR usage. I think it is maybe not suitable (out of the box) and apparently needs to be controlled via an SPI interface. The seller I think is based in China and despite their claims to produce arduino (STM32) code "on request" ... it ain't happening I think. I am not an "electronics or programming guy", so is there some code somewhere out there?
Thank you all in advance.
NXP offers the BGA3X31 evaluation kit OM17024: DOCSIS 3.1 upstream amplifier BGA3131 customer evaluation kit|NXP .
Kit Contains:
RF evaluation board
USB interface board
Flat cable
Samples
USB flash driver containing: evaluation software, Introduction etc.
ESD safe casing
I am nor sure what bga3031 board you have but we support only our products.
Have a great day,
Andrei
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------