Zigbee 920MHz solution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Zigbee 920MHz solution

1,549件の閲覧回数
DonnyChiu
Contributor II

We are looking for a Zigbee solution that runs at 920MHz (Japan variation).

It will just be an addition feature to our existing product.

Seems Freescale has solution for 2.4GHz with the KW20 series.

But I wonder if it works and if it is ready on the KW01 series too.

0 件の賞賛
返信
2 返答(返信)

1,291件の閲覧回数
jasonchiang
NXP Employee
NXP Employee

KW01 is already launched and can be used for 920MHz.

0 件の賞賛
返信

1,291件の閲覧回数
AlanCollins
Contributor V

FSL does have MKW01x operable in 920MHz. FSL also supports 802.15.4e/g standard for this device. However, the ZigBee stack is not yet implemented on MKW01x.

0 件の賞賛
返信