ZigBee data acknowledge problem. Confirm Status = not enough memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ZigBee data acknowledge problem. Confirm Status = not enough memory

ソリューションへジャンプ
2,237件の閲覧回数
Elisa
Contributor III

I want to send packets using


afAddrInfo.txOptions = (gApsTxOptionNone_c | gApsTxOptionAckTx_c)


and


status = AF_DataRequest(&afAddrInfo, mypktPacket, pkt, &myconfirmId);


If status is gZbSuccess_c, I wait the  confirmation.


_______


If I receive a gZbSuccess_c  I will wait and then send a new pkt (frequency is 5 pkt per seconds)


If I receive a gApsNoAck_c i will resend the pkt if my circular data buffer is not full.



The problem is that after few minutes the confirmation status became gZbNoMem_c


What does it means? Who has not enough memory? The sender or the receiver node? 

ラベル(1)
  • RF

0 件の賞賛
返信
1 解決策
1,811件の閲覧回数
AlanCollins
Contributor V

Hello Elisa,

     The "AF_DataRequest" will return "gZbNoMem_c" if it failes to allocate the message. The message goes into the SAP that communicates to the lower layer and eventually becomes an OTA message.

This means you are not freeing correctly the messages your application is using.

I recommend you to turn on the message tracking for debugging what's going on: #define MsgTracking_d 1

Then, when you get the "No mem" error, you can check the "MsgTrackingArray" to see the type of messages that have nto been freed correclty.

Cheers,

Alan

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,812件の閲覧回数
AlanCollins
Contributor V

Hello Elisa,

     The "AF_DataRequest" will return "gZbNoMem_c" if it failes to allocate the message. The message goes into the SAP that communicates to the lower layer and eventually becomes an OTA message.

This means you are not freeing correctly the messages your application is using.

I recommend you to turn on the message tracking for debugging what's going on: #define MsgTracking_d 1

Then, when you get the "No mem" error, you can check the "MsgTrackingArray" to see the type of messages that have nto been freed correclty.

Cheers,

Alan

0 件の賞賛
返信