XQ1TXH5 charge problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

XQ1TXH5 charge problem

1,002 次查看
milimhuang
Contributor I

Hi Sir,
We use your company's NXQ1TXH5 produced in week45 of 2002 and stop charging when the current slowly rises above 1A.

Your company's answer is as follows:

---------------------------------------------------------------------------------------------------------------

Customer could start with those steps to narrow down what is causing the fault: 

(Try each one individually, (after each go back to configuration before changes.)

 

  1.      Replace resistor connected to CNF1 pin with short, 0 Ohm.

This will turn off SPR static power reduction and SPL smart power limiting. 

 

  1.      Replace resistor connected to CNF3 pin with short, 0 Ohm.

This will turn off FOD foreign object detection.Wireless Connectivity

 

  1.      Short NTC pin to ground.

This will turn off external NTC sensing and 85 deg C power reduction threshold.

 ---------------------------------------------------------------------------------------------------------------- 
However, these tests are not improved.
I short NTC3 pin to ground and it can charge.
What is the correct solution?

0 项奖励
回复
0 回复数