Writing flash with user data on MPC5554

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Writing flash with user data on MPC5554

3,713 次查看
dranne
Contributor I

I need to write user data on the internal flash of MPC5554, is there any special code to do that, how can I do this. Please help on this.

 

Regards

dranne

0 项奖励
回复
7 回复数

2,497 次查看
dayve
NXP Employee
NXP Employee

Hey Dranne,

 

Drivers are provided for the device for flash programming and EEPROM emulation.


You can download them and the documentation from the website. From the home page - > 32-bit MCUs -> MPC55xx --> MPC5554.  Select the software and tools tab. You will find the drivers you require here. There are apps note and other resources available as well. .

 

Regards,

Dayve

0 项奖励
回复

2,497 次查看
SABK
Contributor I

the driver you have mentioned does not run for all the versions of mpc5554. how do find out which version is my mpc???

0 项奖励
回复

2,497 次查看
dranne
Contributor I

Ok thanks, I hope these will compile with the Freescale code warrior.

 

Regards

dranne

0 项奖励
回复

2,497 次查看
Bloodhound
Contributor I

Referring to the MPC5566 ref manual, Page 13-26 gives a step by step guide on how to do this.

 

0 项奖励
回复

2,497 次查看
dranne
Contributor I

I want to do In-Application programming of flash, also EEPROM emulation, can you please help on this. Any sample codes or application notes?

 

Thanks in anticipation.

dranne

 

0 项奖励
回复

2,497 次查看
Bloodhound
Contributor I

No not really, apart from pointing you to the app note from Freescale.

0 项奖励
回复

2,497 次查看
dranne
Contributor I

Can you please give me the application note. I'll be very thankful.

 

Also please tell me if I want to run the application from the internal SRAM, how can I do that, I mean program the flash with the application code, then at run time the application is copied to SRAM and execute from there, any idea.

 

Thanks in anticipation.

dranne

0 项奖励
回复