Write error issue -MC13224

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Write error issue -MC13224

1,094 Views
chandrashekarp
Contributor I

Hi all,

We are using free-scale controller MC12334  in our application, initially few baords  we manually assembled and tested . it was working fine.

But as a first of mass production we assembled 200 board  we used Pick plcae .but after the assembly majority of boards are failing to program the controller.

When we trying JTAG  it showing "Write error" when we contacted with assebly house they says they have prepacked with 120 degree for 7 hours(Controller and Bare PCB).

Reflow temperature profile  also same as recommended by freeescale.

Can you please answer few my doubts

1) Write error meaning controller internal flash corrupted or it can be JTAG contact issue with JTAG connector?

2) Prebaking 7 hours at 120 degree is recommended?

Thanks.

chandra

0 Kudos
Reply
0 Replies