Write error issue -MC13224

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Write error issue -MC13224

1,093件の閲覧回数
chandrashekarp
Contributor I

Hi all,

We are using free-scale controller MC12334  in our application, initially few baords  we manually assembled and tested . it was working fine.

But as a first of mass production we assembled 200 board  we used Pick plcae .but after the assembly majority of boards are failing to program the controller.

When we trying JTAG  it showing "Write error" when we contacted with assebly house they says they have prepacked with 120 degree for 7 hours(Controller and Bare PCB).

Reflow temperature profile  also same as recommended by freeescale.

Can you please answer few my doubts

1) Write error meaning controller internal flash corrupted or it can be JTAG contact issue with JTAG connector?

2) Prebaking 7 hours at 120 degree is recommended?

Thanks.

chandra

0 件の賞賛
返信
0 返答(返信)