Which byte lanes are used from the DDR-Controller in the...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which byte lanes are used from the DDR-Controller in the...

跳至解决方案
1,840 次查看
admin
Specialist II
Which byte lanes are used from the DDR-Controller in the MPC8378 in 32 Bit-Mode - MDQ63 to MDQ32 or MDQ31 to MDQ0? MECC's shall be the same  - i think

Thanks for any tip
0 项奖励
回复
1 解答
1,259 次查看
genuap
NXP Employee
NXP Employee
Lower order bits [0:31] should be used.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,260 次查看
genuap
NXP Employee
NXP Employee
Lower order bits [0:31] should be used.
0 项奖励
回复