Which Linux BSP version I should use?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which Linux BSP version I should use?

2,838件の閲覧回数
jpong
Contributor I

I have M9328MX1ADS/M9328MXLADS Ver 2.0 development board, but I don't know which Linux BSP version I should use? 0.3.6 or 0.3.8?

 

Thanks!

0 件の賞賛
返信
3 返答(返信)

1,958件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

It should be 0.3.8 for rev 2.0 board.

 

Actually you should consider using mainline kernel code instead of such very old kernel.

 

Regards,

 

Fabio Estevam

0 件の賞賛
返信

1,958件の閲覧回数
jpong
Contributor I

Thanks Fabio.

 

I have another question. I cannot do the programming bootloader, kernel and rootdisk.

After the bootloader menu show up on screen, for example I choose "0" - programming bootloader, it said "USB drive ready for transfer", then I connect the USB cable with PC and ADS board. The new USB removable will appear in Windows. However, when I drag the file to removable drive, one error message appear on screen and said "cannot copy, please sure the path and filename".

 

Could you please help to tell me which step I made wrong or what problem of my board.

 

Thanks!

0 件の賞賛
返信

1,958件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Sorry, I don't have this board to reproduce this. You can write to Freescale support (www.freescale.com/support) for assistance.

 

Also, you would better use U-boot as your bootloader.

 

Regards,

 

Fabio Estevam

0 件の賞賛
返信