VR5510 cannot enter INIT_FS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VR5510 cannot enter INIT_FS

8,363件の閲覧回数
QR
Contributor I

The board enter debug mode after power up, value of FS_OVUVREG_STATUS is 0x5550, then write 1 to clear the flag, the value of FS_OVUVREG_STATUS keeps 0, and RSTB output high, the FS0B output low,and then make the device go to INIT_FS by setting GO_TO_INITFS (bit10 of FS_SAFE_IOS), then get FS_STATES,the FSM_STATES(FS_STATES[4:0]) always is 0x05, but there is not any information about 0x05. how to get the VR5510 to enter the INITFS?

 

0 件の賞賛
返信
13 返答(返信)

8,345件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

1:FS_OVUVREG as 0x5550 mean VCORE and VDDIO have UV error,you need eliminate them firstly then to power on.

2:You can see below flow chart,after LBIST/ABISL1 no more issue,it will automatically enter into INIT phase.

guoweisun_0-1681714700641.png

 

0 件の賞賛
返信

8,342件の閲覧回数
QR
Contributor I
UV flags cleared only one time, the flags keeped 0, and UV flags have not been setting again. FS_DIAG_SAFETY is 0x040f, LBIST and ABIST always ok.
is the cause is the UV error?
0 件の賞賛
返信

8,339件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You should double check the UV error on VCORE and VDDIO.

Then RSTB assert to high,FS0B assert high?

what do you mean FSM_STATES(FS_STATES[4:0]) always is 0x05? can you double check it again?

 

0 件の賞賛
返信

8,331件の閲覧回数
QR
Contributor I

VCORE is 1.807v, VDDIO is 3.287v. it is ok.
RSTB assert to high,FS0B assert low.

 I'm sure that FSM_STATES(FS_STATES[4:0]) always is 0x05

QR_0-1681718299075.png

Does the status of FS0B prevent the device from entering INIT_FS?

0 件の賞賛
返信

8,327件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

After pass the LBIST and ABISL1,the SBC enter into INIT phase automatically which mean no need send the register of GOTO_INITFS bit.

0 件の賞賛
返信

8,322件の閲覧回数
QR
Contributor I

thank you.

I try to get the FS_STATES without writting GO_TO_INIT, it didn't work. the state is still 0x05.

0 件の賞賛
返信

8,314件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

what about don't enter into debug mode only normal operation?

guoweisun_0-1681779634126.png

 

0 件の賞賛
返信

8,305件の閲覧回数
QR
Contributor I
the same with the last case,it didn't work, the state is 0x05.
0 件の賞賛
返信

8,268件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

你有换过板子测试吗?你的芯片是QM还是ASILB or D是哪个芯片?

0 件の賞賛
返信

8,260件の閲覧回数
QR
Contributor I
上面调试用的是MVR5510AMDALES,是ASIL D的,板子是硬件画的,换过板子,读到的数据是一样的。
刚才用开发板试了下,读到的状态是正常的,开发板使用的型号是MVR5510AMDAHES,也是ASIL D的。
0 件の賞賛
返信

8,243件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

首先你看看板子硬件电路跟EVM 的区别。MVR5510AMDALE BUCk1/2 是single phase,MVR5510AMDAHES BUCK1/2是dual phase

0 件の賞賛
返信

8,171件の閲覧回数
QR
Contributor I

不好意思,之前错看成S32G-VNP-RDB2的原理图导致认为使用的VR5510型号不一致,实际使用的S32G-VNP-RDB3开发板,开发板原理图上标的型号是 PVR5510AMDALES ,实际应该是 MVR5510AMDALES ,这样的话我手上的板子与开发板使用的型号是一致的,我这边再排查看看,感谢!

0 件の賞賛
返信

8,224件の閲覧回数
QR
Contributor I
我手上的板子关于BUCK1/2这块的硬件连接与开发板一致,看到可以通过OTP更改这块的配置,我现在尝试把它改为dual phase看看,谢谢!
0 件の賞賛
返信