Using MC33772CTP2AE with 4 cells

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using MC33772CTP2AE with 4 cells

1,256 Views
hbsantos
Contributor II

Could you provide a reference design using MC33772CTP2AE with 4 cells? Because the reference designs are based on MC33772CTP1AE which uses 3 to 6 cells. I don't know the necessary connections for the circuit to function correctly.

1 Reply

1,232 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello hbsantos,

I hope all is great with you. Thank you for using the NXP communities.

As we know, the MC33772B device can manage up to 6 cells. When fewer than 6 cells are used with MC33772B device, there are connection options for the unused cell controller inputs. Numerous connection options are available.

We do have a document that might be useful for you. In this case, you would need to share with us your active NDA Number.

In case you do not have an NDA, please submit a new case.

I hope this information helps.

Regards,

David

0 Kudos
Reply