Unique ID for MPC5675K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unique ID for MPC5675K

Jump to solution
1,555 Views
mohammedshibin
Contributor I

Hai all,

For my application I need an unique ID since I have more than one board with same MCU.

So I have gone through the data sheet and found Part ID 1(Plant and lot number in ASCII format) and Part ID 2(Wafer number and coordinates).

It is located in Test flash with an offset 0x0058 and 0x0060 respectively.

I need to know whether both Part Id 1 and Part ID 2 are unique or not for a particular controller?

Thank you.

Mohammed Shibin

0 Kudos
Reply
1 Solution
1,424 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have just tried it with 2 devices and I can confirm both values are the same, thus this number is NOT unique.

As I know Unique Device ID is only available with MPC5676R, MPC5674F and MPC5644A (considering MPC56xx) and it is provided by System Information Module.

View solution in original post

0 Kudos
Reply
1 Reply
1,425 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have just tried it with 2 devices and I can confirm both values are the same, thus this number is NOT unique.

As I know Unique Device ID is only available with MPC5676R, MPC5674F and MPC5644A (considering MPC56xx) and it is provided by System Information Module.

0 Kudos
Reply