Unable to program With LPC link2 in IAR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to program With LPC link2 in IAR

1,881 次查看
nxf58908
NXP Employee
NXP Employee

Hello

I am trying to program MKM34x development board using LPC link2 debug probe using one of the SDK demo Application code downloaded from SDK builder. But when I try to debug that code, it shows NO PROBE FOUND error.

I am able to program using MCUXpresso IDE. Also if I make a new project in IAR, I am able to program that as well.

Can Anyone help why I am unable to program that SDK demo code.

Thanks

Madhur Agarwal

0 项奖励
回复
1 回复

1,852 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Madhur Agarwal

Thank you for your interest in the NXP kinetis product, I would like to provide service for you.
When you use the LPC LINK2, what's the debug firmware you are using? CMSIS DAP or JLINK?
Can you firmware your LPC LINK2 debug firmware as JLINK?
Then use the JLINK commander to conect your KM34X board, check whether you can find the ARM core or not.
Just check whether your hardware connection have problems or not.
Please try it.
Any updated information, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复