Unable to access source.codeaurora.org

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to access source.codeaurora.org

8,168 Views
gsureshk
Contributor I

I am trying to compile flexbuild_lsdk2004 for lx2160 processor on the host PC having Ubuntu18.04LTS, then I am seeing below mentioned issue. Please help me to resolve this issue.

Building ATF ...
Cloning into '/home/gsureshk/MyCodes/flexbuild_lsdk2004/packages/firmware/atf'...
fatal: unable to access 'https://source.codeaurora.org/external/qoriq/qoriq-components/atf.git/': Could not resolve host: source.codeaurora.org
/home/gsureshk/MyCodes/flexbuild_lsdk2004/packages/firmware/atf.mk:14: recipe for target 'atf' failed
make[1]: *** [atf] Error 128
make[1]: Leaving directory '/home/gsureshk/MyCodes/flexbuild_lsdk2004/packages/firmware'
Makefile:19: recipe for target 'atf' failed
make: *** [atf] Error 2
make: Leaving directory '/home/gsureshk/MyCodes/flexbuild_lsdk2004'

0 Kudos
Reply
5 Replies

8,129 Views
mahonr59
Contributor I

did you resolve this? because i'm having the same problem

0 Kudos
Reply

8,143 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Please take a look on the following Post that also applies to layerscape devices

Linux source code migration (CAF -> Github) - NXP Community

BR.

0 Kudos
Reply

8,082 Views
gsureshk
Contributor I

HI Oswalag,

I have gone through your explanation, but still I could not able to build flexbuilder_lsdk2004 for LX2160ARDB_REV2.

Could you please give me some steps to build flexbuilder_lsdk2004 for lx2160ardb_rev2 through flex-builder command without directing to source.codeaurora.com

Thanks & Regards

Suresh

0 Kudos
Reply

8,036 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Please download the latest updated version from the following link and try again, it must work fine.

Layerscape Software Development Kit - Updated to pull from GitHub insteadof CodeAurora repository

 

BR, 

Oswaldo

0 Kudos
Reply

8,017 Views
gsureshk
Contributor I

Hi Oswalag,

flexbuild_lsdk2108_github.tgz only migrated from source.codeaurora to Github. But we are looking for flexbuild_lsdk2004/flexbuild_lsdk2004_updated_290520 and these versions not migrated to Github yet.

Any how I can able to compile my flexbuild_lsdk2004_updated_290520 by modifying the build_lsdk.cfg file.

Here is the modified build_lsdk.cfg (build_lsdk.txt should be converted to build_lsdk.cfg), this file has to be replaced in the folder flexbuild_lsdk2004_updated_290520/configs. I could able to build the code for LX2160ARDB_REV2,  with attached build_lsdk.cfg,

Thanks & Regards

Suresh

0 Kudos
Reply