Unable to Train Model on own datasets via eIQ Toolkit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to Train Model on own datasets via eIQ Toolkit

1,235 Views
JKTan
Contributor II

Hi,

 

I would like to train a model using own dataset via eIQ Toolkit. I had conformed my dataset to the VOC dataset format mentioned in eIQ Toolkit. Here is a screenshot of my dataset. My dataset image size is fixed at 640x640.

JKTan_0-1724725848366.png

However, when I proceed to training of the model, the following errors show up. The settings are all the default settings that eIQ Toolkit. I did not change any parameter.

JKTan_1-1724725931016.png

JKTan_2-1724725952168.png

 

FYI, I selected "Detection > Balanced > NPU" for my model. I also tried with other available models, but all failed. How to resolve?

4 Replies

1,221 Views
jimmychan
NXP TechSupport
NXP TechSupport

Which product are you using?

0 Kudos
Reply

1,218 Views
JKTan
Contributor II

Hi,

 

I am using i.MX8MPlus EVK board. By my understanding, eIQ Toolkit should be product independent, right?

 

Regards,

JK

0 Kudos
Reply

1,203 Views
jimmychan
NXP TechSupport
NXP TechSupport

Could you send me the dataset? so I could try it on my side.

0 Kudos
Reply

1,187 Views
JKTan
Contributor II
0 Kudos
Reply