Unable to Train Model on own datasets via eIQ Toolkit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to Train Model on own datasets via eIQ Toolkit

2,104件の閲覧回数
JKTan
Contributor II

Hi,

 

I would like to train a model using own dataset via eIQ Toolkit. I had conformed my dataset to the VOC dataset format mentioned in eIQ Toolkit. Here is a screenshot of my dataset. My dataset image size is fixed at 640x640.

JKTan_0-1724725848366.png

However, when I proceed to training of the model, the following errors show up. The settings are all the default settings that eIQ Toolkit. I did not change any parameter.

JKTan_1-1724725931016.png

JKTan_2-1724725952168.png

 

FYI, I selected "Detection > Balanced > NPU" for my model. I also tried with other available models, but all failed. How to resolve?

4 返答(返信)

2,090件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which product are you using?

0 件の賞賛
返信

2,087件の閲覧回数
JKTan
Contributor II

Hi,

 

I am using i.MX8MPlus EVK board. By my understanding, eIQ Toolkit should be product independent, right?

 

Regards,

JK

0 件の賞賛
返信

2,072件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Could you send me the dataset? so I could try it on my side.

0 件の賞賛
返信

2,056件の閲覧回数
JKTan
Contributor II
0 件の賞賛
返信