USB open failure with CodeWarrior TAP on Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB open failure with CodeWarrior TAP on Linux

Jump to solution
7,315 Views
Rinke
Contributor II

Hi all,

 

I am having issues with connecting to my CodeWarrior TAP using CCS.

0: USB open failure
There are no command converters configured

 

I found the resolution document and I have tried all steps. I made the empty 80-net-name-slot.rules file. I can see the TAP when executing findcc cwtaps.

Rinke_0-1723237950974.png

I can see the TAP in dmesg

Rinke_1-1723237980539.png

It has an ip address

Rinke_2-1723238000070.png

And I can ssh into it

Rinke_3-1723238022738.png

 

So it should be connected right? No...

When checking with ccs

I get the USB open failure. How do I resolve this?

 

 

 

0 Kudos
Reply
1 Solution
7,163 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached workaround to use CodeWarrior TAP USB connection in Linux OS.

View solution in original post

0 Kudos
Reply
9 Replies
7,244 Views
Rinke
Contributor II
Anyone have any tips?
0 Kudos
Reply
7,164 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached workaround to use CodeWarrior TAP USB connection in Linux OS.

0 Kudos
Reply
7,110 Views
Rinke
Contributor II

That does not change anything. Any other tips?

0 Kudos
Reply
7,090 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please provide the step by step result according to document Resolution.docx

0 Kudos
Reply
7,065 Views
Rinke
Contributor II

Hey,

 

If you look at my main post it already contains screenshots of the stuff asked/checked in your document.

0 Kudos
Reply
6,921 Views
pb3
Contributor II

Just out of curiosity - have you managed to solve this issue?

0 Kudos
Reply
6,889 Views
Rinke
Contributor II
Yes! Sorry for the late reply. For me indeed I found out I was configuring it wrongly. Following the document closely works.
0 Kudos
Reply
6,919 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to my document.

0 Kudos
Reply
7,048 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please provide step 4 and step 5 results according to my document.

You need to use CodeWarrior TAP Ethernet configuration as the workaround, please use the IP address of CWTAP usb0 ethernet interface.

0 Kudos
Reply