UJA1168 Error frame

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UJA1168 Error frame

2,407 Views
yi_wang1
Contributor I

Hello NXP Team,

          I use UJA1168TKVXFD in my project, but it appear error frame when we do ESD test(±15kv). If there are some good solution can fix this issue?

  

         Thank you!

         BR.

, 

Labels (6)
0 Kudos
Reply
1 Reply

2,320 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Wang,

Please note that the UJA1168 only supports ±8 kV ESD (HBM), ±15 kV is not guaranteed. However, you can try to add choke or clamp circuit (e.g. the PESD1CAN) between CANH/CANL.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 Kudos
Reply