The issue with the clock output from the SMA port marked as RXC_TX_TCLK on the TJA1103EVB evaluation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The issue with the clock output from the SMA port marked as RXC_TX_TCLK on the TJA1103EVB evaluation

80件の閲覧回数
shilinli
Contributor I

Due to the inability to access the data sheet of the automotive PHY chip corresponding to TJA1103EVB, there are currently some issues in the purchasing process. From the available EVB user manuals, there is no description of the output of the SMA port marked as RXC_TX_TCLK. Therefore, I would like to ask if the output clock is 25 MHz or 66.66 MHz? I referred to another TJA1101BHN/0Z chip, and the description of the 17th pin TXCLK in the data sheet is "transmit clock output in test mode and during slave jitter test", so I am guessing whether the SMA output marked as RXC_TX_TCLK on TJA1103EVB is 25 MHz or 66.66 MHz? If it can be determined, I will be able to make a decision on purchasing.

0 件の賞賛
返信
1 返信

47件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hello @shilinli ,

on pin 26 - RXC/GPIO8/TX_CLK - there is 25MHz in RGMII mode and in MII mode.

Requested documentation for this product is under control release, accessible under NDA (Non-Disclosure Agreement) via Secure Files.

Please Request Access here: https://www.nxp.com/webapp-signup/docstoreReg

Please note, during the form submission you will be asked to upload valid NDA copy. If your company does not have any yet please fill the form for NDA first:
https://www.nxp.com/webapp-signup/ndaReqForm

When NDA is ready you can request secure files access

Kindly check FAQs to understand the process:
https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS
https://www.nxp.com/support/support/secure-access-rights/secure-access-rights-faqs:SEC-ACCESS-FAQS

Best regards,

Pavel

0 件の賞賛
返信