The Yocto build doesn't boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The Yocto build doesn't boot

1,989件の閲覧回数
AKL123
Contributor I

I've the board EVB-SCMIMX6SX. It works fine with the demo SD-CARD.

I compiled the yocto project with the following arguments
DISTRO=fsl-imx-waylandimx6sxsabresd
MACHINE=imx6sxsabresd


Then I used the command
zstdcat imx-image-core-imx6sxsabresd.rootfs-20241028154829.wic.zst | sudo dd of=/dev/sd<partition> bs=1M conv=fsync
to copy the wic file to a spare SD card (8G).

The copy was successful (i.e. no errors displayed), but the board didn't boot.

How can I solve this problem?
Am I using the wrong values for the DISTRO/MACHINE arguments?

0 件の賞賛
返信
3 返答(返信)

1,957件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using the NXP i.MX 6SoloX SABRE Development Board | NXP Semiconductors board? If yes, you can use this MACHINE=imx6sxsabresd.

And here you need to check if the boot mode are set to boot from SD card firstly.

0 件の賞賛
返信

1,911件の閲覧回数
AKL123
Contributor I

My board is EVB-SCMIMX6SX. Please confirm if the MACHINE=imx6sxsabresd works with it.

Kindly find attached the boot_messages.txt captured from the original sd-card that came with the board.

Linux_Distro.png

0 件の賞賛
返信

1,894件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

This is the board :

Rita_Wang_0-1731467618821.png

 

 

For the boar in your hand is :

Rita_Wang_2-1731467463524.png

They are not the same board, so can not use the same name.

linux-imx/arch/arm/boot/dts at imx_4.14.98_2.2.0 · nxp-imx/linux-imx · GitHub

 

0 件の賞賛
返信