TV Input / Video Input interface to imx31

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TV Input / Video Input interface to imx31

5,509 Views
madhu_slf
Contributor I
Hi All,

Has anyone used TV tuner card or a video input device with imx31?
I am trying to use a tv tuner card with imx31. I want to know which tv tuner card i can use and the which driver and application i can use for it.


Thank you,
Madhu
0 Kudos
Reply
5 Replies

2,458 Views
madhu_slf
Contributor I
Hi,

I am trying to get TV-out interface on MX31L. I am using FS453 daughter card for this purpose. I have done the electrical connections from MX31L to FS453 card. also there is a driver provided with the linux source for FS453. THe driver is able to detect the card through I2C. But i'm not getting any output from the card on display. I just got a default color bar and some flickering video out on display but it is not smooth and consistant.
Has anyone worked on this? Please help.


Thank you,
Madhu
0 Kudos
Reply

2,458 Views
SG96
Contributor I

Did you already compile the drivers for the TV tuner card. I am also trying to use a USB TV tuner card from ATI/AMD but did not have much luck compiling the drivers for iMX27.

Are you using the standard BSP from freescale.

0 Kudos
Reply

2,458 Views
ADUBOST
Contributor I
Hi,
I use a Video decoder (TVP5150) on my iMX27, and it works very fine !
I think the video input port is the same on iMX31
Bye



Message Edited by ADUBOST on 2008-06-25 01:24 PM
0 Kudos
Reply

2,458 Views
harald_krapfenb
Contributor III

@ADUBOST:

 

Do you have Linux running on the i.MX27 for the TVP5150 decoder?

 

Greetings,

Harry

 

0 Kudos
Reply

2,458 Views
madhu_slf
Contributor I
Hi,

I am using imx31L and trying to interface a USB2.0 tv tuner/ video input adapter.
Has anyone used USB2.0 tv tuner/ video input adapter? Any success with that?
I am planning to use hauppauge wintv usb2. has anybody used this?

Looking forward for positive replies and successful works.

Thanks,
Madhu


0 Kudos
Reply