TSS Freemaster Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TSS Freemaster Question

848件の閲覧回数
haroldvogel
Contributor II

Receive that following warning 'missing braces around initializer' TSS_Freemaster.C

the code is:

 

#if FMSTR_USE_TSA

 

/* FreeMASTER TSA table for TSS variables */


//FreeMASTER interface to write



FMSTR_WRITE_STRUCT)

 

FMSTR_WRITE_STRUCT, indexdata,       FMSTR_TSA_UINT32)

 

FMSTR_WRITE_STRUCT, flagreg,         FMSTR_TSA_UINT32)

 

FMSTR_CONFIG_STRUCT)

 

FMSTR_CONFIG_STRUCT, ptr_size,       FMSTR_TSA_UINT8)

 

FMSTR_CONFIG_STRUCT, low_bit_mask,   FMSTR_TSA_UINT8)

 

//TSS system config menu


TSS_CSSystem)

 

TSS_CSSystem, Faults,                       FMSTR_TSA_UINT8)

 

TSS_CSSystem, SystemConfig,                 FMSTR_TSA_UINT8)

 

TSS_CSSystem, NSamples,                     FMSTR_TSA_UINT8)

 

TSS_CSSystem, DCTrackerRate,                FMSTR_TSA_UINT8)

 

TSS_CSSystem, SlowDCTrackerFactor,          FMSTR_TSA_UINT8)

 

TSS_CSSystem, ResponseTime,                 FMSTR_TSA_UINT8)

 

TSS_CSSystem, StuckKeyTimeout,              FMSTR_TSA_UINT8)

 

TSS_CSSystem, LowPowerElectrode,            FMSTR_TSA_UINT8)

 

TSS_CSSystem, LowPowerElectrodeSensitivity, FMSTR_TSA_UINT8)

 

TSS_CSSystem, SystemTrigger,                FMSTR_TSA_UINT8)

 

// Keydetector 2 data


#if (TSS_USE_KEYDETECTOR_VERSION == 2)

 

#endif


//electrodes config menu


#if TSS_USE_DELTA_LOG

 

#endif


#if TSS_USE_SIGNAL_LOG

 

#endif


#if TSS_USE_INTEGRATION_DELTA_LOG

 

#endif


#if ((TSS_USE_NOISE_MODE == 1) && (TSS_USE_NOISE_SIGNAL_LOG == 1))

 

#endif


//controls menu


#if TSS_N_CONTROLS > 0

 

#endif


// TSS version information


#endif

 

Not sure if I should put a ';' after each function or what should be done.  This is code that I received from TSS application.

 

I have attached the file.

Original Attachment has been moved to: TSS_Freemaster.c.zip

0 件の賞賛
返信
0 返答(返信)