TJA1145 interrupt on RXD question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1145 interrupt on RXD question

2,366件の閲覧回数
freddy_ben-zeev
Contributor IV

We're considering using TJA1145. The product datasheet says that it uses the RXD signal for interrupt to the MCU. RXD is also the CAN input signal to the MCU. Can such an interrupt happen during normal operation or only in standby and sleep modes? If it can happen in normal operation how do I tell the difference between interrupt and CAN RX data?

Thanks,

Freddy

タグ(1)
2 返答(返信)

2,267件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi Freddy,

it can happen only in Standby or Sleep modes, in normal mode RXD has CAN bit stream.

pastedImage_1.png

BR, Petr

2,267件の閲覧回数
freddy_ben-zeev
Contributor IV

Thanks. I thought so but I wanted to be sure.

0 件の賞賛
返信