TJA1145 interrupt on RXD question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TJA1145 interrupt on RXD question

2,347 次查看
freddy_ben-zeev
Contributor IV

We're considering using TJA1145. The product datasheet says that it uses the RXD signal for interrupt to the MCU. RXD is also the CAN input signal to the MCU. Can such an interrupt happen during normal operation or only in standby and sleep modes? If it can happen in normal operation how do I tell the difference between interrupt and CAN RX data?

Thanks,

Freddy

标记 (1)
2 回复数

2,248 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi Freddy,

it can happen only in Standby or Sleep modes, in normal mode RXD has CAN bit stream.

pastedImage_1.png

BR, Petr

2,248 次查看
freddy_ben-zeev
Contributor IV

Thanks. I thought so but I wanted to be sure.

0 项奖励
回复