TJA1145 interrupt on RXD question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1145 interrupt on RXD question

2,387 Views
freddy_ben-zeev
Contributor IV

We're considering using TJA1145. The product datasheet says that it uses the RXD signal for interrupt to the MCU. RXD is also the CAN input signal to the MCU. Can such an interrupt happen during normal operation or only in standby and sleep modes? If it can happen in normal operation how do I tell the difference between interrupt and CAN RX data?

Thanks,

Freddy

Tags (1)
2 Replies

2,288 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Freddy,

it can happen only in Standby or Sleep modes, in normal mode RXD has CAN bit stream.

pastedImage_1.png

BR, Petr

2,288 Views
freddy_ben-zeev
Contributor IV

Thanks. I thought so but I wanted to be sure.

0 Kudos
Reply