TJA1080 Termination

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1080 Termination

780 Views
kiran_m1
Contributor I

what is the termination resistor required for Flexray transceivers TJA1080ATS

0 Kudos
Reply
3 Replies

684 Views
kiran_m1
Contributor I

If I am not using split termination(like in figure below) is it ok to put Rbus=94 ohms in between BP and BM? Or is Rbus=47 ohms?

pastedImage_1.png

0 Kudos
Reply

684 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can put Rbus=94 ohms but still suggest use the split termination!

0 Kudos
Reply

684 Views
guoweisun
NXP TechSupport
NXP TechSupport

For the bus termination it is highly recommended to use the so-called split termination.

Split termination is able to significantly improve the signal symmetry between BP and BM, thus reducing electromagnetic emission and improving electromagnetic immunity.

Recommended values for the split termination capacitor are within the range from 4.7nF to 47nF.

The value of the two resistors should match at least within 2% (absolute tolerance 1%).
At those two nodes that have the maximum electrical distance on the bus it is recommended that the cable ends are terminated with a resistance equal or slightly higher to the nominal cable impedance, e.g. RT/2 = 47Ω.

At all other nodes it is possible to use a high-ohmic termination with e.g. RT/2 = 1300Ω.

0 Kudos
Reply